AXIS#.IL.LIMITP
Description
This parameter sets the positive user limit clamp value of the torque-producing q-component current command (AXIS#.IL.CMD ). The current command is additionally limited by the motor peak current setting (AXIS#.MOTOR.IPEAK ) and by the present value of the foldback I²t peak motor current protection.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
A |
|
Range |
0 A to drive peak current (IPEAK) |
|
Default Value |
Drive peak current (IPEAK) |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.LIMITP |
500ah |
04h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.IL.LIMITP |
510ah |
04h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5814 |
1 |
5814 (0x16b6) |
AXIS1.IL.LIMITP |
Signed32 |
Read/Write |
Yes |
|
71350 |
2 |
5814 (0x16b6) |
AXIS2.IL.LIMITP |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.IL.LIMITP |
5814 |
Float |
Read/Write |
- |